NumericFunctions.Square root
Returns the square root of a numeric expression
Format
ANSI-SQL Format:
SQRT( Expr )
ODBC Format:
{{ FN SQRT( Expr ) }}
Remarks
Returns the square root of Expr. Expr can be any numeric expression. If Expr is negative a run time error is reported.
Example:
SQRT( 64 )
{FN SQRT( Value )}